Case studies

Tate's Attiro flooring for LAYER project in Belgium

Tate provides premium magnetic wood flooring for the LAYER project in Waterloo, Belgium

  • Sector: Commercial office
  • Location: Waterloo, Belgium
  • Completion date: September 2025
  • Architect: Luc Spits

Blending elegance with functionality, the LAYER project in Waterloo stands as a modern icon of innovation and design. This new construction, completed in 2024, leverages cutting-edge sustainable technologies to create a sophisticated workspace that offers style combined with flexibility. A key element in achieving this is Tate's Attiro magnetic flooring system, installed throughout the building to deliver both aesthetic appeal and practical functionality.

The LAYER building showcases contemporary architecture, designed to accommodate flexible workspaces and dynamic environments. To meet the needs of a constantly evolving workspace, the design team selected Tate's Attiro system – a real wood, magnetically-backed flooring solution that is as beautiful as it is functional. With its quick and easy access to the underfloor void, Attiro allows for effortless reconfiguration of the space, making it ideal for modern office workspaces.

The beauty of magnetic timber flooring

Attiro's unique design features engineered oak staves that magnetically attach to Tate's encapsulated steel raised access floor panels. This allows the floor to be lifted easily with a specialised device, providing fast access to underfloor services such as electrical wiring and HVAC systems. The magnetic system ensures that panels can be lifted and replaced without disruption, making maintenance and reconfiguration seamless.

The flooring is available in a variety of shades and finishes, including brushed, sawmill, and rustic hand-scraped options, allowing for customisation to suit the building’s design. Attiro’s durability is ensured through a hard wax oil finish, which enhances the natural beauty of the European oak veneer while offering protection against wear.

Versatility and efficiency

Attiro was installed in LAYER during the final fit-out phase, streamlining the construction process and reducing lead times. Its versatility makes it perfect for the dynamic environment of the LAYER building, where office layouts and furniture arrangements may need frequent changes. The ability to access the underfloor void with minimal effort makes it easy to reconfigure the workspace as needed, contributing to an uncluttered and flexible working environment.

Attiro’s combination of style and practicality makes it an ideal choice for modern buildings that prioritise both design and functionality. As seen in the LAYER project, it helps to create a refined yet adaptable environment, ready to meet the challenges of the future.

United Kingdom & Ireland enquiries:

+44 (0) 1482 781701

Burma Drive
Hull
HU9 5SG
United Kingdom

© 2025 Kingspan Group. All Rights Reserved

*We have achieved Cradle to Cradle Certified® Silver for these Raised Access Flooring Panels under certification number 7236. Cradle to Cradle Certified® is a registered trademark of the Cradle to Cradle Products Innovation Institute. Cradle to Cradle Certified® is the world's most advanced science-based, multi-attribute certification program for designing, making and verifying materials and products that are safe, circular and responsibly made.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.