Knowledge articles

PSA performance specification – Setting the standard for raised access floors

The PSA: 2021 specification for raised access floors, or PSA MOB PF2 PS/SPU 2021 to give it its full title, gives architects and specifiers confidence in the longevity and sustainability of the products they choose for their new-build, renovation and fit-out projects.

The PSA: 2021 specification for raised access floors, or PSA MOB PF2 PS/SPU 2021 to give it its full title, gives architects and specifiers confidence in the longevity and sustainability of the products they choose for their new-build, renovation and fit-out projects.

The PSA: 2021 spec is the long-standing go-to standard of testing for raised access floors in the UK & Ireland for 3 key reasons:

  • PSA-grade raised access floors are independently tested and verified
  • The PSA offers a simple pass or fail
  • The PSA guarantees a full 25-year warranty

Ultimate performance, leading standards

PSA: 2021 is the de facto specification for raised access floors in the UK & Ireland. Compared to the equivalent European standard EN 12825: 2001, the PSA: 2021 specification, grades and testing methods are the benchmarks for raised access flooring within high-performance buildings.

How does this compare to the EN specification?

  • The EN 12825: 2001 has 72 performance standards, which architects and specifiers find confusing and open to misunderstanding.
  • The EN 12825: 2001 only accounts for vertical loading, unlike the PSA which is far more extensive. As well as that, the EN 12825: 2001 ignores pedestal heights.
  • With EN 12825: 2001, there is no independent testing. It is down to each manufacturer to test and self-certify, which is open to bias, misinterpretation and incorrect information.
  • Under the PSA Standard: 2021 all products must be guaranteed for 25 years. With EN 12825: 2001, no guarantee is required.
How they differ PSA EN 12825
Independently tested and certified
25 year system guarantee
Clear guidance on loads & suitable applications
Highest quality safety & performance

How is the PSA: 2021 a more comprehensive testing procedure?

To achieve a PSA: 2021 grade, a raised access floor system must undergo a series of stringent independent testing procedures, which includes analysis of:

  • Structure
  • Loadings
  • Weight
  • Hygrothermal properties
  • Fire and safety
  • Acoustic performance
  • Use of floorcoverings
  • Electrical requirements
  • Contaminant effects
  • Durability
  • Transportation
  • Installation

The result of a PSA: 2021 test is either a pass or fail and very clear in terms of performance, strength and suitability. By choosing an access flooring system with a PSA: 2021 specification, architects get unsurpassed testing to safeguard their client's investment and ensure the ultimate in long-lasting performance.

PSA:2021 hygrothermal properties testing

Contact our specifications team

Our team has helped countless architects & specifiers achieve the best possible raised access flooring performance using the leading PSA standards. Specifications Team  today to discuss your project on +44 (0) 1482 781701

United Kingdom & Ireland enquiries:

+44 (0) 1482 781701

Burma Drive
Hull
HU9 5SG
United Kingdom

© 2025 Kingspan Group. All Rights Reserved

*We have achieved Cradle to Cradle Certified® Silver for these Raised Access Flooring Panels under certification number 7236. Cradle to Cradle Certified® is a registered trademark of the Cradle to Cradle Products Innovation Institute. Cradle to Cradle Certified® is the world's most advanced science-based, multi-attribute certification program for designing, making and verifying materials and products that are safe, circular and responsibly made.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.