David Churchill

Knowledge articles

The future of the office: Transforming the world of work

The design of office work environments is at the centre of a critical discussion about how companies should adapt to a rapidly evolving workplace.

The design of office work environments is at the centre of a critical discussion about how companies should adapt to a rapidly evolving workplace.

New work practices and the rapid advancement of digitalisation across many business operations have fundamentally reshaped the employee experience and led to a re-evaluation of traditional office layouts.

And although no one is entirely sure what the office of the future will look like, it’s widely agreed that a well-designed working area will support and improve teamworking, as well as enhance company culture.

Technology advancements are allowing companies to become more flexible, agile and support cross-team collaboration – the latter being particularly important for those adopting the hybrid working model (where employees spend at least 2-3 days/week in the office) where physical daily contact may be more limited. Rather than this reducing productivity, we’re seeing how investment in IT can support employees wherever they are based and enable seamless co-working.

Offices are being reconfigured to promote and support the new ways of working. Demand is rising for offices that are smaller, to accommodate a lower headcount at any one time, and more flexible, and companies are prioritising more face-to-face contact through initiatives such as creating more communal spaces in office buildings.

But that’s not the only trend. Recognising that offices are inevitably being compared to ‘home comforts’ for those used to working in their home office, many companies are improving on-site leisure, health, and well-being facilities, as well as investing in smarter decor.

In major financial centres, such as London, this is being taken a step further. Smaller offices means there has been more money to spend on luxury office accommodation - or, as The Economist reports - we’re seeing the rise of the uber-luxurious office.

Is this a long-term trend? It may be one that is at the mercy of macro-economic trends - recessions and downturns have a habit of reining in any spending deemed to be non-critical. But there is little doubt that younger generations are more attracted to companies that focus on employee well-being, and talent will out.

What about sustainability?

For many businesses, sustainability is as important as an improved employee experience with great emphasis placed on minimising environmental impact, waste reduction, and the use of lower carbon materials in construction.

However, while new build standards are mandated, most offices are housed in ageing buildings which were built at a time when energy efficiency standards were considerably below where they are now.

According to a report published by Carter Jonas: Offices: Past, Present, Future in April 2023, around a fifth of the UK office space fails to achieve current energy efficiency ratings that allows them to be let – that’s an Energy Performance Certification of at least E – although the report indicates that this figure may need to be treated with caution because some buildings will be exempt, and others may be being modified. Oxford, Cardiff and Edinburgh were reported as having the largest percentage of low rating offices, while only 28 per cent of the country’s office stock was rated high quality – which is, as we’ve discussed, where the demand is currently highest.

As the report’s authors note: “Occupiers are demanding office space that meets increasingly high sustainability criteria. This is partly being driven by legislation such as the minimum energy efficiency standards (MEES) legislation.

“Increasingly, however, the drive towards sustainable space is being driven by occupier preferences, with many corporates placing this high on their list of property selection criteria.

“In the current competitive labour market, providing a vibrant, attractive, and sustainable work environment is increasingly important for the recruitment and retention of talent, encouraging working from the office, and promoting the well-being of employees. In addition, high energy prices have made the benefits of an energy-efficient building all the more apparent.”

Citi Bank – flexible, inspiring, net zero building refurbishment

Office refurbishment projects are, not surprisingly, extremely popular at the moment. Transforming existing office spaces into new workplaces, focused on improved user experience, and with low embodied carbon, are features of many of our most recent projects.

At Citi Bank’s Canary Wharf offices, we were contracted to support a project to reinvigorate the company’s 20-year-old office building as part of a full interior renovation.

The project delivered an agile, inspiring space that supports modern, hybrid, working practices and delivers against Citi Bank’s net-zero commitment.

It was conceived as a highly flexible space which could be quickly reconfigured to meet the needs of employees when they are in the office. As well as smart design, the renovations make innovative use of technology to drive cross-team creativity and collaboration.

It features Tate Hollow Floor, a system which is ideally suited to high-traffic areas. This tough, impact-resistant flooring can be used as a complementary system alongside floors which use steel-encapsulated panels - such as the RMG600+.

Both systems can be partnered with virtually any floor finish, including carpet, laminate, timbers, or vinyl, to create beautiful, inspiring designs.

Typically, Tate’s floor panels contain up to 75% recycled content without any compromise on their strength, integrity, or aesthetic quality. Plus, they are covered by our 25-year manufacturer’s warranty and fully tested to PSA: 2021 standards. We have a popular Take Back Scheme for any offcuts or waste material from our product, which we then recycle, ensuring they don’t end up in landfill.

We provide certified performance data, and verified environmental credentials and production claims, which are fully backed by independent evaluations and industry standards.

The project is due to be completed in 2025.

Products used in this project

United Kingdom & Ireland enquiries:

+44 (0) 1482 781701

Burma Drive
Hull
HU9 5SG
United Kingdom

© 2025 Kingspan Group. All Rights Reserved

*We have achieved Cradle to Cradle Certified® Silver for these Raised Access Flooring Panels under certification number 7236. Cradle to Cradle Certified® is a registered trademark of the Cradle to Cradle Products Innovation Institute. Cradle to Cradle Certified® is the world's most advanced science-based, multi-attribute certification program for designing, making and verifying materials and products that are safe, circular and responsibly made.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.