Case studies

Full Structural Refurbishment of Original Canary Wharf Office

Canary Wharf’s 30 South Colonnade, now known as YY London demonstrates its sustainability efforts through its building design and function. Everyone involved had the responsibility of making sure this development became a new landmark of London.

  • Sector: Commercial Office
  • Location: Canary Wharf, London
  • Completion date: September 2023
  • Architect: Buckley Gray Yeoman
  • Products: RMG600

This was a unique commercial office refurbishment project. A waterfront location, a distinctive façade, and located in the heart of Canary Wharf. Our close collaboration with Skanska has delivered a modern, sustainable building, located in the heart of London’s vibrant Canary Wharf community.

Commercial office

Structural refurbishment & new office construction

Demonstrating sustainability through design

Working with main contractor, Skanska, the Tate team helped find a raised access flooring solution for the challenges they faced, resulting in the customer’s bespoke requirements being met.

Talk to us find out more

A primary feature of this development is the giant floor-to-ceiling windows with a Y-shaped curved façade. This guaranteed that the 37,000 sq. m. of PSA:2021 medium grade RMG600 access flooring by Tate was a dynamic feature in its own right and complemented the professional office surroundings whilst remaining functional and adaptable. Tate raised access floor systems can be raised one panel at a time for precision and functionality when making required alterations in the underfloor void.

Supreme redesign, sustainably built for wellbeing

Like other projects in this area, harnessing innovation and being at the forefront of sustainability was important. Their sustainability objectives can be seen through many aspects of the development beginning at the design to the physical functionality and usage.

Installing our raised access floor systems in this development helped enable the office refurbishment to achieve a BREEAM Outstanding sustainable building certification. Two different systems were used for this project and both are supported by Environmental Product Declarations (EPD) that showcase these systems. The latest version of RMG600 (2023) has just 1.67 kg of CO2e per panel in modules A1 – A3 (product stage) of the product life cycle impact assessment (EN15804:2012 + A2:2019 update). The fusion of first-class design features with the retention of the existing structure, together with the sustainability efforts of this project have ensured that the development has achieved an overall saving of 10,260 tonnes of CO2.

The access floor systems that were used in this project were RMG600 and FDEB_H. RMG600 is a PSA:2021 Standard medium-grade system used in offices and FDEB_H is a PSA:2021 Standard heavy grade access floor used in data, IT, and plant rooms within the building.

The FDEB system is finished with a resilient surface covering that includes a High Pressure Laminate (HPL) architectural finish to control static. For this project, HPL was chosen because of its suitability within server rooms with a high volume of electrical equipment. Its intrinsic properties that dissipate static electricity make it extremely safe for these environments. It is also highly durable and resilient whilst still providing an attractive finish.

Gathering Inspiration from Location

It was a fantastic opportunity to be involved in a prestigious development in the heart of London’s Canary Wharf. The sustainability credentials of the building align with our own long-term Planet Passionate sustainability initiatives.

This development offers a cost-effective Environmental, Social and Governance (ESG) alternative to constructing new commercial buildings.

Products used in this project

Find out more about the products used in this project below.

United Kingdom & Ireland enquiries:

+44 (0) 1482 781701

Burma Drive
Hull
HU9 5SG
United Kingdom

© 2025 Kingspan Group. All Rights Reserved

*We have achieved Cradle to Cradle Certified® Silver for these Raised Access Flooring Panels under certification number 7236. Cradle to Cradle Certified® is a registered trademark of the Cradle to Cradle Products Innovation Institute. Cradle to Cradle Certified® is the world's most advanced science-based, multi-attribute certification program for designing, making and verifying materials and products that are safe, circular and responsibly made.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.

Tate logo

Our products are installed in the most prestigious buildings in the UK and across the globe. We are working to reduce our carbon footprint, introduce fully recyclable access floor panels, improve our manufacturing processes and maintain the highest standards as we support the development of sustainable commercial offices.

The visual and acoustic impact that an engineered wood floor has on commercial spaces is unsurpassed. Genuine wood flooring delivers a warmth, comfort and quality combining natural timbers with the practical, flexible features of an innovative raised access floor.